Toshiba Satelitte L455-S5975 problem! help me??

Reply
Member
Posts: 3

Toshiba Satelitte L455-S5975 problem! help me??

Hi Toshiba People,

 

I have the Satelitte L455-S5975 laptop. Had it since December 2009. A few weeks ago, it wanted me to do the windows updates (computer was being slow) so i went to do the updates and once the computer shut off it will not turn on again. I have the laptop a/c cord plugged in and all it does is light up above the cord logo on the computer. Nothing else happens at all. Im missing two keys, one doesnt work and i have to go to the windows keyboard to make it work and the other the plastic piece wont go back on.

 

Anyone else have this problem? What can I do to fix it?

Super Advisor
Posts: 4,069

Re: Toshiba Satelitte L455-S5975 problem! help me??

[ Edited ]

For the startup problem try this. Power off your computer, unplug the AC adapter, remove the battery, press and hold down the power button for 30 seconds, replace the battery and AC, power the unit on, if it starts, as soon as you see the Toshiba logo, press the 'F2' key to enter the BIOS Setup, in setup press 'F9' to load setup defaults, then press 'F10' to save and exit, try to let it boot into Windows.

 

Satellite Laptop Keyboard V000120240

 

Laptop key replacement & tutorial

 

Check your private messages here.

 

Mike

 

 

Member
Posts: 3

Re: Toshiba Satelitte L455-S5975 problem! help me??

tired that but it still wouldnt work.